TGML File Format
TGML (TAC Graphics Markup Language) is a declarative XML-based language for dynamic 2D graphics.
Graphics created in Graphics Editor are saved as .TGML files.
When you create a graphic in Graphics Editor, a TGML root object is created at the bottom of the Objects tree in the objects pane. The TGML root object is also the default layer in the work area of Graphics Editor. The TGML object cannot be deleted.
For more information, see the following sections: